This is model US1GC30B. If it’s recoginized by BIOS and I boot to it that way it works fine. However if I include the provided drivers in boot.wim and boot from a USB image the adapter fails intermittently. You can see it frequently drop the link light on the switch. I’ve loaded the drivers provided on the support page for this adapter into the boot.wim included on the USB thumb drive.
Specifically what I’m doing is creating a discover image in WDS via known working setup image. I used “copype” for copy of Win PE files. then used “makewinpemedia” to create a bootable USB drive. I then took the boot discover wim file and injected the startec drivers provided on the support page. Copied this file over to the sources folder replacing the existing boot.wim file.