Stuck with 107b-usb-hdmi and macbook air m3 2024

Im a newibie, i bought the 107b-usb to drive 2 ext screens with clam open. I have followed instructions and downloaded drivers which seems to load an app called macosinstantview now display link video adaptor. when I get to the part where I need to connect the monitor the instant view app doesn’t seem to recognise that the monitor its plugged in. Any suggestions. thanks

Hi @ilan and thank you for posting on our StarTech.com Community!

I am sorry to hear that you are having issues getting your 107B-USB-HDMI adapter working there. I will provide some troubleshooting that could help with resolving this issue.

If both of these have been confirmed, testing the adapter on another computer is a great test to confirm if the issue is somehow related to the adapter, or computer. Depending on the outcome, I would then highly suggest reaching out to one of our Technical Advisors via our livechat who would then be able to assist further with some real time troubleshooting to assist in finding a resolution for this issue. You can find the livechat link on our website at www.startech.com.

Sincerely,
@AdamS