Hi,
I am experiencing a reproducible display issue with a StarTech 132UE-TB4USB4DOCK connected to a MacBook Pro with Apple M1 Pro.
The dock works normally during regular use. The problem occurs after the displays have gone to sleep.
My normal setup is:
- MacBook Pro with Apple M1 Pro
- StarTech 132UE-TB4USB4DOCK connected via Thunderbolt 4
- Two external LG displays, both connected to the dock via HDMI
- MacBook normally used in clamshell mode
- Apple USB keyboard connected through the dock
- Ethernet and an external USB-C drive also connected to the dock
- Power Delivery provided by the StarTech dock
The issue is consistently reproducible with the following sequence:
- Everything is working normally and both external displays are active.
- I lock macOS and wait for the displays to turn off.
- I wake the Mac using the external keyboard and unlock it.
- Both external displays initially wake up and work normally.
- Approximately 3 seconds after wake/unlock, both external displays go black.
- Power-cycling the StarTech dock immediately restores normal operation.
I performed several tests to determine whether this was a macOS sleep issue or a loss of the Thunderbolt connection.
The Mac itself does not go back to sleep.
I repeated the test with the MacBook lid open. When the problem occurred, the built-in MacBook display continued to work normally and the session remained unlocked, while only the displays connected through the StarTech dock went black.
macOS still detects the external displays while they are black.
During the failure, System Settings > Displays continues to show both external monitors. I also captured system_profiler SPThunderboltDataType SPDisplaysDataType while the problem was occurring. Both LG displays were still reported as: Online: Yes
The StarTech dock was also still detected and the Thunderbolt/USB4 connection remained active at 40 Gb/s.
Other dock functions, including USB devices and Ethernet, also continue to operate. Therefore, the dock itself does not appear to disconnect from the Mac; only the video output stops working.
The problem also occurs with only one HDMI display connected to the StarTech dock.
I disconnected one of the two HDMI displays and repeated the test. The remaining display still became black approximately 3 seconds after wake. Therefore, the problem does not appear to require a dual-display configuration.
I then performed an A/B test using another dock that I previously used with this Mac: a Kensington UH1400P USB-C dock.
I connected:
- one external display through the StarTech 132UE-TB4USB4DOCK;
- one external display through the Kensington UH1400P;
- both docks to the same MacBook Pro at the same time.
I then repeated exactly the same lock/display-sleep/wake procedure with the MacBook lid closed.
After wake:
- the display connected through the Kensington continued working normally;
- the display connected through the StarTech became black after approximately 10 seconds.
The MacBook remained awake and usable through the display connected to the Kensington dock.
This is particularly relevant because, before purchasing the StarTech dock, I used two Kensington UH1400P adapters simultaneously, one for each external HDMI display, with the same MacBook and the same monitors. I did not experience this wake issue with that configuration.
I also checked the StarTech dock information reported by macOS. system_profiler currently reports:
Product: 132N-TB4USB4DOCK
Mode: USB4
Firmware Version: 41.1
Micro Firmware Version: 0.88.0
Link Speed: 40 Gb/s
I would therefore appreciate your help determining whether this is a known sleep/wake or display reinitialization issue with the 132UE-TB4USB4DOCK on Apple Silicon/macOS, and in particular:
- Is firmware 41.1 / micro firmware 0.88.0 the latest firmware available for this dock?
- Are there any firmware updates addressing display wake, HDMI output, DisplayPort tunneling, or Apple Silicon compatibility?
- Is there any diagnostic information I can collect from macOS while the dock is in this failed state that would help your engineering/support team investigate the issue?
- Are there any known compatibility issues with this dock and Apple M1 Pro systems after display sleep?
I can reproduce the issue consistently and would be happy to provide system_profiler output or perform additional diagnostic tests if required.
Thank you.