When I run the Movavi Video Editor SE after installation and entering the key, and attempt to capture, I get this screen. image at Imgur: The magic of the Internet
The camera (runcam 3) works if connected directly to a device composite video connector, like a tv.
The svidusb232 is connected between the RunCam and the USB port sn 0324010782, is warm and the green light is on. The latest driver from your web has been installed.
I’ve also tried IOTA video capture 2.4d. it gives the screen i sent earlier (Device “USB 2828x Device” cannot be used for video capture).
Clearly, I’m doing something wrong or have left out a step. However, I’ve followed the very simple instructions in the pamphlet that came with the svidusb232, two software disc and also the online SVID2USB232_usermanual.pdf
Kenneth Drake