That one does not appear to support 720x400 @ 70hz btw, per the response of the agent here. There are few alternatives that work with that specific and important resolution and refresh rate. If you want a good and sure solution then you should definitely go with the adapter that says that it will support it.
If you are pursuing other possibilities, then avoid anything that does not have that input on their full specs sheet. I have found that omissions of that particular input are intentional and not due to it being old, and any adapter missing it (not listed on full product specifications sheet) do not support it. I have been bitten by this several times with cheap products from amazon. None of them appear to support 720x400@70hz. I know of a sure 3, 2 being very expensive. The last one works and is rather compact, but it it can only be found on the rare occasion that it is on sale used. I am unsure if I am able to state what it is on this site however, as this is a startech forum. I might have to ask about that. It could be seen as advertising.
Hopefully you can find one, from one tech to another. I signed up to this forum to respond so that you can hopefully avoid my mistakes. I spent many hours down this rabbit hole looking for a vga to hdmi adapter that worked after I found out all of the cheap ones didn’t actually work for bios lol. GL!